VBUS.UVMODE

Description

VBUS.UVMODE sets what happens when the under voltage, UV, condition is detected. An under voltage is triggered:

When VBUS.UVMODE = 0, an undervoltage fault is issued whenever the DC bus voltage, VBUS.VALUE, goes below the fault threshold, VBUS.UVFTHRESH.

When VBUS.UVMODE = 1, an undervoltage fault is issued whenever the DC bus voltage, VBUS.VALUE, goes below the fault threshold, VBUS.UVFTHRESH and the controller attempts to enable the drive (software or hardware enable).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

See Also

VBUS.VALUE, VBUS.UVFTHRESH
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
VBUS.UVMODE

300ah

04h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

VBUS.UVMODE

2512

9D0

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.UVMODE

2512

Unsigned8

Read/Write

-